Optional Intermediate Repository (IR) Database (DB) Configuration
Optional Intermediate Repository (IR) Database (DB) Configuration
APM Connect allows dynamic configuration for both data extraction from your EAM system and the configuration of APM data pushed back into your EAM system from APM. This configuration is achieved by manipulating table entries in the Intermediate Repository Database (IRDB).
CAUTION: As you will be editing the IRDB table entries, it is recommended to take a backup of the existing database so that it can be restored in the event the changes you make do not have the desired effect. The backup can be of the entire database that you are modifying.
Database Backup Steps
Procedure
Database Restoration Steps
Procedure
Northbound & Southbound Data Extraction SAP Mapping Configuration
To facilitate a dynamic mapping capability for data extracted from SAP and pushed into APM, the below IRDB tables can be configured. The structure of the tables and fields that are modified during configuration is outlined in subsequent sections of the documentation.
- autoextractor_control
- autoloader_control
- autojoin_control
- southbound_mapping_control
Within each table are rows that correspond with steps for data extraction to support the following data types:
- Asset Strategy Integration
- Equipment
- Equipment Technical Characteristics
- Functional Location
- Functional Location Technical Characteristics
- Planned Work Interface
- Static Data
- Work Management Interface
- Work History
Northbound Data Integration Data Flows
During the northbound data integration, each interface follows the following logic:
Southbound Data Integration Data Flows
During the southbound data integration, each interface follows the following logic: