Deployment Steps
Step 1 - Setup Environment
Procedure
Step 2 - Setup Atom
Procedure
Results
- A new service
Atom
is available underServices.msc
. - In platform, Atom with status Online will be attached to your selected environment.Note: For more details on the Atom configuration options, refer to the Boomi Documentation available in the Remote Management platform.
Step 3 - Install Integration Pack
Procedure
- In the platform, select Deploy and select Integration Packs.
- On the right side of the window, select the Browse Integration Packs button.
- A list of the Releases assigned to your account will be displayed. Select the latest release number.
- Then, select the View button and then select Install.
- In the Choose New Process Name (optional) field, provide the baseline release number (by default) or the custom name for your custom projects. Then, select Complete Installation.
- When the Integration Pack is installed, select Close.
- The installed Integration will be listed in the leftmost panel as shown in the screenshot below.
- Select the previously installed Integration pack from the leftmost panel.
- In the Attached Environments and Unattached Environments fields, select the test environment from the Unattached Environment list (which you have created in Step 1 – Setup Environment)
- Then, select <<Attach Selected button to move the selected Integration pack from left Unattached Environment list to Attached Environment list. The Integration pack will now be attached to your selected Environment.
- The selected Environment will now appear on the Attached Environment list for the Integration pack.
Step 4 – Setup/Configure Connection Settings
Procedure
Step 5a - Execute a Process Manually
Procedure
- In the platform, select Manage and then select Process Reporting.
- Click Execute Process and, in Select an Atom field, select your Atom under the appropriate environment.
- Then in the Process field, select the process under your installed Integration Packs, which you want to execute, and select the Execute button.
- A record against your execution will be displayed.
- View or save the logs by selecting the File icon.