Configure Filters in Visualizations
Configure Date Filters using Reporting Objects
Before You Begin
- Ensure that you are part of the Security Groups available for users within this module, to manage Advanced Visualization.
For more information on the roles and groups available for the Advanced Visualization users, refer to the topic.
About This Task
When visualizing data in a dashboard, you can configure a custom date range as filter criteria to view data for the specified period. However, you can configure the date filters using a reporting object so that the date filters appear on the dashboard by default. For more information on the reporting objects, refer to the help integrated with Advanced Visualization.
This topic describes how to configure the date filters using a reporting object.
Procedure
Configure Filters on a Dashboard using a GE Digital APM Query
Before You Begin
- Make sure that the catalog query that you want to use for populating filter parameters is valid and returns the correct set of values.
About This Task
Advanced Visualization enables you to use a data source to populate filter parameters for filtering a dashboard created for another data source. The data sources are created using GE Digital APM queries. You must use a query that retrieves a set of values from the GE Digital APM database, which can be used as the filter parameters.
For example, you have created a dashboard to visualize work order details, such as work order ID, asset, work order status, and so on. Each of these parameters may have multiple values. If you want to filter the dashboard with work order types which are not a part of the fields list returned by visualization data source, you will need to create a filter using the work order type field available in a separate data source. You must populate the work order type filter with the values coming from this separate data source so that you can specify filter criteria. To populate the values, you will need this separate data source that can be associated with the first data source used for visualizing work order details.
This topic describes how to configure a filter and populate filter parameters using a data source created for a GE Digital APM query.
Procedure
- Access the Advanced Visualization page.
- Perform the following steps to create and configure the data source for populating filter parameters in the filter:
- Perform the following steps to configure the filter on the dashboard: