Deployment
Deploy Advanced Visualization for the First Time
GE Digital APM delivers an installation package that includes files needed for a successful implementation of Advanced Visualization. The topics outline the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic GE Digital APM system architecture.
About This Task
Task | Notes |
---|---|
Open the required server ports. | This step is required. |
Review the Advanced Visualization system requirements. | This step is required. |
Review the database requirements. | This step is required. |
Run the Advanced Visualization Installer. | This step is required. |
Required Server Ports
To provide communication between Advanced Visualization and other systems, make sure the listed ports are open.
Port Numbers | Description |
---|---|
80, 8005, 8080, 8120, 9090 | Used by Advanced Visualization User Interface. |
9006 | Used by Advanced Visualization User Interface. This port is required only if Advanced Visualization is installed on the same machine as GE Digital APM. |
System Requirements
License Requirements
This feature is available with the core GE Digital APM application; no specific license is required.
Hardware Requirements
The following hardware requirements outline the minimum hardware required for any computer that will be set up for Advanced Visualization. These minimum requirements may not be sufficient, depending upon how your system is configured and the anticipated user load the system must service.
Component | Minimum Requirements |
---|---|
Core |
4-core processor, 2.5 GHz minimum per core 8-core processors are recommended for optimal performance |
RAM | 16 GB RAM or higher for optimal performance |
Hard Drive | 40 GB of free disk space |
Software Requirements
The following software is required on any machine that will be set up for Advanced Visualization.
Software Name and Version | Where you can obtain it |
---|---|
Windows Server 2012 (64-bit) or Windows Server 2016 (64-bit) or Windows Server 2019 (64-bit) | Microsoft |
Browser | Notes |
---|---|
Google Chrome or Mozilla Firefox or Microsoft Edge | For recommended browser versions, refer to the TIBCO browser information. |
Database Requirements
You must create a database before installing Advanced Visualization. Advanced Visualization supports the following relational databases.
- PostgreSQL
- Microsoft SQL Server
- Oracle
Database Provider | Requirements |
---|---|
Microsoft SQL Server |
|
Oracle |
|
Advanced Visualization Installation Steps
Before You Begin
Before you can run the Advanced Visualization installer, you must:
- Ensure that your system meets the system requirements.
- Ensure that you have access to the Advanced Visualization installation package.
- Ensure that you can access the APM Server host URL from the server where you plan to install Advanced Visualization.
About This Task
Procedure
Results
What To Do Next
Uninstall Advanced Visualization
This procedure uninstalls APM Advanced Visualization after the initial installation.