Data Sources
About Advanced Visualization Data Sources
Advanced Visualization provides out of the box capabilities that enable you to visualize data for the following GE Digital APM features and modules:
- Baseline entities and queries
- General recommendations
Each of these features is associated with a set of data sources in Advanced Visualization. The data sources contain a set of logically related fields that allow you to create and customize the visualizations based on the access privileges that you have for the specific feature.
Note: Although you have access to all the data sources, you must also have access to the required capabilities to create visualizations using these data sources. . You can visualize the data for the assets based on the security groups and roles assigned to your GE Digital APM user account.
The following table provides high-level information about the data sources available for the supported modules or features:
Module/Feature | Data Source Description |
---|---|
General Recommendations | You can visualize data based on the general recommendations data available within GE Digital APM. |
GE Digital APM Baseline Queries | You can visualize data using the baseline query views available in GE Digital APM. Note:
|
Create a Data Source using a GE Digital APM Query
Before You Begin
- Make sure that the baseline query or the custom query that you want to use to create a data source exists in the Catalog.
About This Task
This topic describes how to create a data source using a baseline query or a custom query, and configure the data source to enable the Advanced Visualization users to create charts or dashboards using the data source.
Procedure
What To Do Next
Retrieve Query Details of a GE Digital APM Query using Query Helper
About This Task
When creating a data source using a baseline or custom query, you must have the following query details:
- Sample request body for the Insert (POST) operation
- Service URL extension
- Valid query path
- Valid query parameters and parameter values
This task describes how to retrieve and validate the parameter details of a query to create a data source.