SAP PI Family Fields

EAM System

EAM System records are used to store information about your systems to facilitate data extractions and loads.

When you transfer data from APM to your EAM or service management system, the APM system uses EAM System records to determine which EAM system to use.

In addition, EAM System records are used by the Equipment Adapter and the Functional Location Adapter.

This topic provides an alphabetical list and description of the fields that exist for the EAM System family. The information in the table reflects the baseline state and behavior of these fields.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.

FieldData TypeDescriptionBehavior and Usage
Default EAM System?BooleanA value that indicates whether this system should be used by default when transferring data between your APM system and your system.

On the datasheet, you can select the check box to identify this system as the Default EAM System.

The default EAM system is used when creating a notification from a General Recommendation when there is no technical object from which to obtain the EAM system for the creation of the notification.

NameCharacterThe name of the system.You can enter any name, but we recommend that you enter a name in the format <SYSID>-<CLIENT>, where <SYSID> is the System ID of the system and <CLIENT> is the Client number. By doing so, the value in the Name field will match the value that will be populated automatically in the System ID field.
PasswordCharacterThe password to the system.The password that you enter will be encrypted and displayed as asterisks on the datasheet.
Reconnect DelayNumericSpecifies the delay in seconds between when a communication failure is encountered when connecting and when the system should try to connect again.

The default value is 0.

Enter your unique value.

SAP PI AAEBooleanIf you are using SAP 7.3 or above, you may use the Advanced Adapter Engine (AAE). This parameter allows this functionality to be used during extraction.

You must enter one of the following values:

  • true: If you are using AAE.
  • false: If you are not using AAE. This is the default.
SAP PI HostCharacter The SAP PI server host. Enter your unique value.
SAP PI PortCharacterThe SAP PI server port.Enter your unique value.
SAP PI Receiver PartyCharacter The receiver determined in the communication channel section in SAP. This field is optional. Enter your unique value.
SAP PI Receiver ServiceCharacterThe receiver service determined in the communication channel section in SAP. This field is optional. Enter your unique value.
SAP PI Sender PartyCharacterThe receiver sender determined in the communication channel section in SAP. This field is optional. Enter your unique value.
SAP PI Sender ServiceCharacterThe sender service determined in the communication channel in SAP.The default value is GE_APMConnect.
System IDCharacterThe ID of the system.This field is populated automatically after you test the connection to the system using the Test Connection link on the Associated Pages menu.

Specifically, the System ID field is populated automatically with the name of the system, using the format <SYSID>-<CLIENT>, where <SYSID> is the System ID of the system and <CLIENT> is the Client number.

System TypeCharacterEAM system type.Enter the value SAP_PI.
User IDCharacterThe User ID of a user that can log in to the system.None