Automated Data Loader Service Installation

Install Automated Data Loader Service

The Automated Data Loader service required for integrating to APM using Automatic Data Loader (ADL) is configured as part of the Southbound Service installation. To use only the ADL, execute the Southbound Service and Postgres installation only. You do not require a remotely managed runtime environment for ADL to function.

Create ADL directories

The following table lists the directories that must be created when using the ADL.

Considerations:
  • The folders must be created in the directory specified in the southbound configuration file (see ADL Configuration).
  • Create the directories only for the Data Loader types that are in use.
Note: By default, all the Data Loader Types have the same processing priority of 99 (prefix). This can be changed to get precedence in the processing. For example, 01˜FamilyDataLoader.
Data Loader NameFolder Name
Family Data LoaderFamilyDataLoader
Equipment and Functional Location LoaderEquipmentFunctionalLocationLoader
Taxonomy Data LoaderTaxonomyLoader
Work History LoaderWorkHistoryLoader
Production Loss Analysis (PLA) 1 - AdminPLAAdminBatchDataLoader
Production Loss Analysis (PLA) 2 - EventPLAEventBatchDataLoader
Production Loss Analysis (PLA) 3 - PlanPLAPlanBatchDataLoader
Root Cause Analysis (RCA)RCABatchDataLoader
System Reliability Data LoaderSystemReliabilityBatchDataLoader
Asset Criticality Analysis (ACA Checklist)ACACheckListDataLoader
Asset Criticality Analysis (ACA)ACAMatrixDataLoader
GIS Data LoaderGISDATALOADER
Policy Instance Data LoaderPolicyInstanceBatchDataLoader
Role Data LoaderRolesDataLoader
Rounds Allowable ValuesAllowableValuesBatchDataLoader
Rounds ReadingsReadingsBatchDataLoader
Rounds RoutesRouteBatchDataLoader
Rounds Templates and Template GroupsTemplateBatchDataLoader
Inspection Management (IM) AssetsIMBatchAssetDataLoader
Inspection Management (IM) Functional LocationIMBatchFLDataLoader
RBI Components To TML Groups RelationshipRBITMBatchDataLoader
Risk Based Inspection (RBI) 580RBI580BatchDataLoader
Risk Based Inspection (RBI) 581RBI581BatchDataLoader
Risk Based Inspection (RBI) Corrosion LoopRBICorrosionLoopBatchDataLoader
Thickness Monitoring (TM) EquipmentTMBatchAssetDataLoader
Thickness Monitoring (TM) Functional LocationTMBatchFLDataLoader
Thickness Monitoring (TM) Piping EquipmentTMBatchPipingAssetDataLoader
Thickness Monitoring (TM) Piping Functional LocationTMBatchPipingFLDataLoader
Generation Availability Analysis (GAA) GADS Amplification CodesGAAAmplificationCodeDataLoader
Generation Availability Analysis (GAA) GADS Cause CodeGAACauseCodeDataLoader
Generation Availability Analysis (GAA) EventsGAAEventsDataLoader
Calibration ManagementCalibrationBatchDataLoader
Hazard AnalysisHazardAnalysisBatchDataLoader
Asset Strategy Management (ASM)AsmDataLoader
Asset Strategy Management (ASM) TemplateAsmTemplateDataLoader
Failure Modes and Effects Analysis (FMEA)FMEAAnalysisDataLoader
Failure Modes and Effects Analysis (FMEA) Analysis TemplatesFMEAAnalysisTemplateDataLoader
Failure Modes and Effects Analysis (FMEA) Asset TemplatesFMEAAssetTemplateDataLoader
Reliability Centered Maintenance (RCM)RCMAnalysisDataLoader
Reliability Centered Maintenance (RCM) Analysis TemplateRCMAnalysisTemplateDataLoader
Risk MatrixRiskMatrixDataLoader
GAA Wind Asset HierarchyGAAWindAssetHierarchyDataLoader
GAA Wind EventsGAAWindEventDataloader
GAA Wind Sub Group CapacityGAAWindSubgroupCapacityDataLoader
Rounds Pro - Picklist DataloaderPicklistDataloader
Rounds Pro - Route Master DataloaderRouteMasterDataloader
Rounds Pro - Step DataloaderStepDataloader
Rounds Pro - Step ConditionsStepConditionDataloader
Rounds Pro - Step TemplateStepTemplateDataloader