Deploy the APM on a Windows Mobile Device for the First time
Deploy APM on a Windows Mobile Device for the First Time
The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Note: If you are deploying this module in APM Now, before you begin completing these tasks, review the system requirements for this module to identify the supported features for this module in APM Now. Unless noted, all deployment tasks in the following table are applicable for the deployment of this module in APM Now.
APM Sync Server
Note: APM Sync Server is only required if you want to use Operator Rounds on Windows Mobile handheld devices.
Step | Task | Notes |
---|---|---|
1 | Configure the APM Sync Server. Configuring the APM Sync Server includes completing the following steps.
| This step is required only if you want to use Operator Rounds on Windows Mobile handheld devices. |
2 | Configure security for the MeridiumSyncService Service. | This step is required only if you want to use Operator Rounds on Windows Mobile handheld devices. |
Windows Mobile Handheld Device
the following tasks need to be performed on each Windows Mobile handheld device that you want to use with Operator Rounds.
Step | Task | Notes |
---|---|---|
1 | Ensure that all the Windows Mobile handheld devices that you want to use with Operator Rounds meet the software requirements. | This step is required. |
2 | Install the .NET Compact Framework. | This step is required. |
3 | Install Microsoft SQL CE. Install Microsoft SQL CE. | This step is required. |
4 | Install Microsoft Sync Services for ADO.NET. | This step is required. |
5 | Install the GE Digital APM Mobile Framework. | This step is required. |
6 | Access Device Settings Screen. | This step is required. |
7 | Identify the Sync Server within the APM Mobile Framework. | This step is required. |
8 | Specify the security query to be used with the APM Mobile Framework. | This step is required. |
9 | Modify the user time-out value. | This step is required. |
10 | Install Operator Rounds. | This step is required. |
11 | Configure barcode scanning. Configuring barcode scanning includes the following steps:
| This step is required only if you will use an Barcode scanner with Operator Rounds. |
12 | Configure RFID tag scanning. Configuring RFID scanning includes the following steps:
| This step is required only if you will use an RFID scanner with Operator Rounds. |
13 | Install translations for Operator Rounds. | This step is only required if you are using translations. |