Create a Custom Device

This topic describes how to create Failure Rate Reference Data for the following types of custom devices:

Steps

  1. Access the SIS Management Overview page.

  2. In the workspace, select the Custom Failure Data tab.

    The Custom Failure Data section appears, displaying a list of Failure Rate Reference Data records for all types of custom devices.

    The Custom Failure Data section

  3. In the upper-left corner of the section, select , and then select the type of the custom device that you want to create.

    A blank custom device datasheet of the selected type appears. The following image shows the datasheet for a Custom Sensor.

    The blank datasheet of a Sensor Custom Device

  4. As needed, enter values in the available fields for the Sensor, Logic Solver, or Final Element.
  5. Select the interfaces, connections, channels, and elements as applicable, and then select Save.

    The custom device is created.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.