Create a Proven In Use Justification Record

Steps

  1. Access one of the following subsystems associated with the device for which you want to create the Proven In Use Justification record:
  2. At the end of the datasheet for the selected subsystem, in the section that contains the list of associated Protective Instrument Devices, select the link in the ID column.

    The Device Details window appears, displaying the datasheet for the selected Protective Instrument Device.

    Device Details window

  3. In the lower-right corner of the window, select Justification Details.

    The datasheet for Proven In Use Justification appears.

    Device Details window

  4. As needed, enter values in the available fields.
  5. In the lower-right corner of the window, select Save.

    The Proven In Use Justification record is created and associated with the device.

    Tip: In the upper-right corner of the window, select to view the datasheet for the Protective Instrument Device.

Copyright © 2018 General Electric Company. All rights reserved.