Protective Instrument Loop records store details about a protective instrument loop that you have created as part of SIL verification. This topic provides an alphabetical list and description of the fields that exist for the Protective Instrument Loop family and appear on the Protective Instrument Loop datasheet by default. The information in this table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Achieved SIL |
Number |
A number representing the overall SIL value for the protective instrument loop. |
This list appears in the Calculated Results section and contains the following options:
For example, if the value in each of these fields is 2, the value in the Achieved SIL field will be 2. If the value in two of the fields is 2 and the value in one of the fields is 1, the value in the Achieved SIL field will be 1. |
Application Test Method | Character | The application test method that is used in the loop. |
This list contains the following options:
These values are defined in the MI_ARCHITECTURE_CONSTRAINT System Code Table. |
Availability |
Number |
A number representing the percentage of time that the protective instrument loop is expected to be available in the case of a demand. |
This field appears in the Calculated Results section and is enabled or disabled based on the following criteria:
Availability = (1-PFD Avg.) *100 |
Calculated SIL | Number | A number representing the SIL value for the protective instrument loop, which is the value stored in the Loop PFD Avg field. |
This field appears in the Calculated Results section and is enabled or disabled based on the following criteria:
|
Calculated SIL Architectural Constraints | Number | The SIL value for the protective instrument loop, which is based on architectural constraints defined in the Test Architecture Constraints field. |
This field appears in the Calculated Results section on the datasheet and is enabled or disabled based upon the following criteria:
|
Calculated SIL Systematic Capabilities | Number |
The SIL value for the protective instrument loop, which is based on systematic capabilities defined in the failure rate data associated with each protective instrument loop element. This is the lowest SIL value among the SIL values of all the elements in the loop. For example, assume that the elements in the loop are capable to achieve the following SIL values:
Then the SIL value for the entire protective instrument loop is 1. |
This field appears in the Calculated Results section and is enabled or disabled based on the following criteria:
|
Calculated STR | Number | A number representing the spurious trip rate for the protective instrument loop. |
This field appears in the Calculated Results section and is enabled or disabled based on the following criteria:
|
Demand Mode | Character |
Represents the estimated probability that a dangerous condition will exist where the instrumented function is required to take the process to its safe state. For instance, if the demand rate is more than once a year, the hazard rate must not be higher than the failure rate. In this case, the SIL mode is high demand or continuous. |
This field is disabled and populated automatically with the value stored in the SIL Mode field in the Instrumented Function that is linked to the Protective Instrument Loop. |
Description | Character | A brief description of the protective instrument loop. | None |
Final Element MCI | Number | A percentage that represents the Maintenance Capability Index. |
This field contains the following options:
|
Last Modified By | Character | The name of the user who last modified the record. | This field is disabled and populated with the name of the GE Digital APM Security User who last modified the Protective Instrument Loop. |
Last Modified Date | Date | The date on which the record was last modified. | This field is disabled and populated with the date on which the Protective Instrument Loop was last modified. |
Logic Solver MCI | Number | A percentage that represents the Maintenance Capability Index. |
This field contains the following options:
|
Loop Class | Character | A value that indicates whether the protective instrument loop is designed to mitigate safety risks or commercial risks. |
This list contains the following options:
|
Loop ID | Character | The ID of the protective instrument loop. | This value is required and must be unique. |
Loop PFD Avg | Number | A number representing the probability that the protective instrument loop will fail in the event of a demand while operating in low demand mode. |
This field appears in the Calculated Results section, which is enabled or disabled based on the following criteria:
|
Loop PFH | Number | A number representing the probability per hour that the protective instrument loop will fail in the event of a demand while operating in high demand or continuous mode. |
This field appears in the Calculated Results section, which is enabled or disabled based on the following criteria:
|
Loop Type | Character | A value representing the category of the protective instrument loop, based on the type of data that the sensor is measuring. |
This field contains the following options:
|
Meets Architectural Constraints? | Character | A value that indicates whether the protective instrument loop's architectural constraints, specified by the standard in the Test Architectural Constraints field, meet the requirement defined by the value in the Required SIL field. |
This list appears in the Calculated Results section and contains the following options:
By default, this value is set to Incomplete.
|
Meets Availability Target? | Character | A value that indicates whether the protective instrument loop's availability meets the availability requirement defined in the Instrumented Function that is linked to the Protective Instrument Loop. |
This list appears in the Calculated Results section and contains the following options:
By default, this value is set to Incomplete.
If the value in the Demand Mode field is High Demand or Continuous, this value is N/A. |
Meets SIL Requirement? | Character |
A value that indicates whether the protective instrument loop's SIL value meets the SIL requirement defined in the Required SIL field. In order to meet the SIL requirement, the values in the following fields must be greater than or equal to the value in the Required SIL field:
|
This list appears in the Calculated Results section and contains the following options:
By default, this value is set to Incomplete.
|
Meets STR Limit? | Character | A value that indicates whether the protective instrument loop's spurious trip rate meets the spurious trip rate requirement defined in the Instrumented Function that is linked to the Protective Instrument Loop. |
This list in the Calculated Results section and contains the following options:
By default, this value is set to Incomplete.
|
Meets Systematic Capabilities? | Character | A value that indicates whether the protective instrument loop's systematic capability meets the systematic capability requirement defined in the Required SIL field. | This list appears in the Calculated
Results section and contains the following options:
This value is set to Incomplete by default.
If the value in the Systematic Capability Validation field is False, this value is set to N/A. |
Mission Time | Number | A number that represents the time that the protective instrument loop or the element will be in use before it is replaced. | This value is measured in years. This value is determined by the least mission time value among the values for all the elements of the protective instrument loop. For example, if the mission time values for the logic solver, final element, and sensor are 10 years, 5 years, and 20 years respectively, then the mission time for the entire loop is 5 years. |
MTTFS | Number | A number that represents the Mean Time To Fail Spuriously (i.e., the mean time until a failure of the loop causes a process trip when a hazard was not present). |
This field appears in the Calculated Results section, which is enabled or disabled based on the following criteria:
This value is measured in years. |
Required SIL | Number | A number representing the SIL value that is required for the protective instrument loop. | This field is disabled and populated with the value stored in the Selected SIL Level field in the Instrumented Function that is linked to the Protective Instrument Loop. |
Risk Reduction Factor | Number | A number representing the factor by which the risk should be reduced for the protective instrument loop. |
This field appears in the Calculated Results section and is enabled or disabled based on the following criteria:
|
Sensor MCI | Number | A value that represents the Maintenance Capability Index. |
This field contains the following options:
|
SIL Verification Method | Character | A value that represents the type of method used to calculate the SIL verification results for the protective instrument loop. |
This field contains the following options:
|
Startup Time | Number | A number representing the amount of time the protective instrument loop has been bypassed since it was in the startup mode. | This value is measured in hours. |
Systematic Capability Validation | Logical | A value that indicates whether the SIL value for the protective instrument loop will account for systematic capabilities, which are defined in the failure data for each protective instrument loop element. | If you select this check box, the protective instrument loop will use systematic capabilities. If you clear this check box, the protective instrument loop will not use systematic capabilities. |
Test Architecture Constraints | Character | A value that indicates the level of safety certification that is associated with the elements in the protective instrument loop. |
This field contains the following options:
|
Copyright © 2018 General Electric Company. All rights reserved.