Failure rate reference data refers to data that exists to record trends in failure rates for categories of elements that exist in a protective instrument loop. These elements can be categorized by application, technology, size, or any other technical characteristic.
Before you add an element to a protective instrument loop, you can consider the failure rate reference data that is associated with that element type, and then make a decision on whether or not to use that particular element.
Validation failure rate reference data is available for the following records:
The Is Reference Data check box in these records is set to True.
Note: By default, the Is Reference Data check box is not included on the datasheet. This field is used by the GE Digital APM system, and is not meant to be modified manually.
When you create a Protective Instrument Loop Element via the Validation Failure Rate Reference Data feature, the GE Digital APM system will automatically select the Is Reference Data check box in that record.
Copyright © 2018 General Electric Company. All rights reserved.