This topic provides an alphabetical list and description of the fields that exist for the Lubricant family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
Lubricant records serve as a means for organizing all the lubricants that are used by your company. When you create a Lubricant record, the values that you enter in these fields will be used to populate the corresponding lists on the Lubrication Requirement datasheet, where you can select the necessary values from a list.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Description | Character | Description of the lubricant. | You can enter a value in this field. |
Flash Point | Numeric | Flash point of the lubricant. | You can enter a value in this field. |
Flash Point UOM | Character | The unit of measurement of the Flash point of the lubricant. |
On the datasheet, this field appears as a list that is populated by the MI_LUBRICANT_REFERENCES system code table. |
ISO Grade | Character | Viscosity grading of the lubricant. | You can enter a value in this field. |
Lubricant | Character | The name of the lubricant. | You can enter a value in this field. |
Lubricant Type | Character | The type of lubricant. |
On the datasheet, this field appears as a list that is populated by the MI_LUBR_TYPE system code table. |
Manufacturer | Numeric | The manufacturer of the lubricant. |
On the datasheet, this field appears as a list that is populated with the values stored in the Manufacturer Name field in existing Lubricant Manufacturer records. This field displays the Manufacturer Name, but stores the Entity Key of the corresponding Lubricant Manufacturer record. If you are creating multiple Lubricant records, you may select the same or different manufacturers for each. |
Manufacturer's Part Number | Character | Manufacturer part number of the lubricant. |
You can enter a value in this field. |
Material Number | Character | Material number of the Lubricant. For example, the material number used in your EAM system. | You can enter a value in this field. |
Notes | Character | Any notes necessary for the lubricant. | You can enter a value in this field. |
Storage Location | Character | Location where the lubricant is stored. | You can enter a value in this field. |
Trade Name | Character | Brand name of the lubricant. | You can enter a value in this field. |
Viscosity Rating | Character | Viscosity index of the lubricant. | You can enter a value in this field. |
Copyright © 2018 General Electric Company. All rights reserved.