The following System Code Tables are used by Rounds:
Table ID |
Table Description |
Function |
---|---|---|
LR_CHAR_POSS_VALS | Possible values for Character type LRs | Used to populate values displayed in Completion Status field when collecting readings for a Lubrication Requirement. |
MI_FDC_STATUS_TYPE |
Status type for Checkpoint families |
NA |
MI_LM_LUBR_REQ_TYPE | Types of Lubrication Requirement | Used to populate the LR Type list on the Lubrication Requirement and Lubrication Requirement Template records. |
MI_LM_REFERENCES | Units of measure for Capacity | Used to populate the Unit of Measure and Capacity Unit of Measure lists in Lubrication Requirement and Lubrication Requirement Template records. |
MI_LUBR_PRIORITY | Lubrication Priority | Used to populate the Priority list in Lubrication Requirement and Lubrication Requirement Template records. |
MI_LUBR_TYPE | Lubricant Types |
Used to populate the Lubricant Type list in Lubricant records. |
MI_LUBRICANT_REFERENCES | Units of measure for Flash Point |
Used to populate the Flash Point UOM list in Lubricant records. This system code table contains a subset of the values in the UOME system code table. |
MI_OPR_MEAS_LOC_TYPE |
List of Measurement Location types |
Used to populate the Measurement Location Type list in Measurement Location records and the Type list on the Operator Rounds Allowable Values page. |
MI_RECOMMENDATION_TYPE |
CORE, Recommendation Type |
Used to populate the Recommendation Type list in Recommendation records. Note that the Recommendation Type field is not included on the baseline OPR Recommendation datasheet. |
MI_TASK_TYPE_REFERENCE |
CORE, Reference values to limit task type lists when creating tasks |
Used to populate the Task Type field in Checkpoint Task records. |
Reading Status |
Reading Status |
Used to populate the Status field in Reading records. |
Route Status |
Route Status |
Used to populate the Status field in Route History records. |
UOME |
Global units of measure list used throughout GE Digital APM |
In Rounds Designer, used to populate the Unit of Measure list in Measurement Location records. |
Copyright © 2018 General Electric Company. All rights reserved.