Lubricant Manufacturer Records

Lubricant Manufacturer records store details about the manufacturer of a lubricant. This topic provides an alphabetical list and description of the fields that exist for the Lubricant Manufacturer family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Manufacturer ID

Character

The ID that you want to use to identify a lubricant manufacturer.

This field is required and must be unique.

Manufacturer Name

Character

The name of a lubricant manufacturer.

This field is required and must be unique.

This field is used to populate the list in the Manufacturer field of Lubricant records.

Manufacturer Description

Character

A description of the lubricant manufacturer.

This field is optional.

Copyright © 2018 General Electric Company. All rights reserved.