This topic describes how to create a Checkpoint Condition and add it to an ML Template Group:
As a successor to an Measurement Location Template whose ML Type value is numeric.
-and-
Steps
The Measurement Location Template node displaying the checkpoint whose reading value should trigger additional checkpoints to appear.
-or-
On the upper-left corner of the pane, select
A new Checkpoint Condition is created and appears below the node representing the selected Measurement Location Template or Checkpoint condition. A blank datasheet for the Condition appears.
In the Select Relation list, select the desired comparator. For example, the following image shows the comparator <= (less than or equal to) selected in the Select Relation list.
In the upper-right corner of the datasheet, select
The Checkpoint Condition is created.
At this point, the Checkpoint Condition node displays part of the final condition statement. In this example, the condition statement is: If the Temperature Reading is less than or equal to 0, then display the following checkpoint.
If you want to create a new Measurement Location Template, select New MLT.
-or-
The Measurement Location Template is added to the ML Template Group, and a Measurement Location Template node appears below the predecessor Checkpoint Condition. A blank datasheet for the Measurement Location Template appears in the workspace.
In the upper-right corner of the datasheet, select
The Measurement Location Template is saved. At this point, the condition statement is complete.
Copyright © 2018 General Electric Company. All rights reserved.