Create a New Measurement Location Template and add to an ML Template Group

This topic describes how to create a Measurement Location Template and add it to a Template Group.

Steps

  1. Access an ML Template Group to which you want to add a Measurement Location.
  2. In the left pane, select the node that will determine the position of the new Measurement Location Template node. For example, if you want a new Measurement Location Template node to appear below an existing Measurement Location Template node, select that existing Measurement Location Template node. In the following image, the last Measurement Location Template node is selected, so the new Measurement Location node will appear below it.

  3. In the upper-left corner of the pane, select , and then select New MLT.

    A new Measurement Location Template node appears in the left pane, and a blank datasheet appears in the workspace.

  4. On the datasheet, in the Template ID box, enter an ID for the Measurement Location Template. This field is required, and the value must be unique.
  5. In the ML Type list, select the value that corresponds to the type of Measurement Location that this Measurement Location Template represents. You can select Character or Numeric.
  6. As needed, enter values in the remaining fields.
  7. In the upper-right corner of the datasheet, select .

    The ML Template Group is saved.

Copyright © 2018 General Electric Company. All rights reserved.