Add a Condition to an ML Template Group for a Character Measurement Location Template

This topic describes how to create a Checkpoint Condition and add it to an ML Template Group:

Steps

  1. Access an ML Template Group.
  2. In the left pane, select:
  3. In the upper-left corner of the pane, select , and then select Condition.

    A new Checkpoint Condition is created and appears below the Node representing the selected Measurement Location Template or the checkpoint condition. A blank datasheet for the Condition appears.

  4. On the Select Value list, select the reading value that should trigger an additional checkpoint to appear.
  5. In the upper-right corner of the datasheet, select .

    The Checkpoint Condition is created. The Checkpoint Condition node displays part of the final condition statement, similar to the one shown in the following image.

  6. In the left pane, select , and:

    The Measurement Location Template is added to the ML Template Group, and a Measurement Location Template node appears below the predecessor Checkpoint Condition. A blank datasheet for the Measurement Location Template appears in the workspace.

  7. As needed, enter or modify values in the available fields.
  8. In the upper-right corner of the datasheet, select .

    The Measurement Location Template is saved. At this point, the condition statement is complete.

Copyright © 2018 General Electric Company. All rights reserved.