Add a Condition to a Route for a Numeric Measurement Location

This topic describes how to create a Checkpoint Condition and add it to a Route:

Steps

  1. Access the Route in which you want to add a Checkpoint Condition.
  2. In the left pane, select:
  3. In the left pane, select , and then select Condition.

    A new Checkpoint Condition is created and appears below the predecessor Measurement Location in the Route pane.

  4. In the Select Relation list, select the desired comparator (i.e. <, <=,=, >=, or >).

  5. In the Select Value box, enter the numeric value representing the reading value that, when combined with the value in the Select Relation box, will trigger the conditional checkpoint to appear.
  6. On the upper-right corner of the datasheet, select .

    The Checkpoint Condition is saved.

  7. In the left pane, select , and then:

    The Measurement Location is added to the Route, and a Measurement Location node appears below the predecessor Checkpoint Condition.

  8. As needed, enter or modify Measurement Location values in the available fields.
  9. On the upper-right corner of the datasheet, select .

    The Measurement Location is saved. The condition statement is complete.

 

Copyright © 2018 General Electric Company. All rights reserved.