The Histogram Plot provides a visual representation of the frequency distribution of the result that you selected in the grid in the Elements section.
Note: Interaction with graphs is not available on touch-screen devices.
The Histogram Plot shows the distribution of the actual values from all iterations that were used to calculate the average value. The distribution of the actual values spreads across a series of data ranges, which are called bins and are represented by columns on the Histogram Plot. When an actual value from an iteration falls into a bin, it is included in the associated column. The higher the column is, the more values have fallen into the bin.
Note: The number of columns that appear in the Histogram Plot is determined by the value in the Histogram Bins field in the root System analysis.
Additional values are represented by the following lines in the Histogram Plot:
Realistic Value: Blue line in the Histogram Plot. This line represents the median value, which is the median value of the values from the iterations of the Scenario.
Note: If the median value falls in between two values, then the larger value will be used as the Realistic value.
Copyright © 2018 General Electric Company. All rights reserved.