Hardware Requirements
The following hardware requirements outline the minimum hardware required for any machine or mobile device that will access the GE Digital APM system. These requirements account for the GE Digital APM software only. Additional hardware may be required on clients where other components are installed. These requirements may not be sufficient, depending upon how your system is configured.
Minimum requirements:
Support for mobile devices is provided in two resolution view modes: full or limited. Full-resolution view mode supports access to the entire GE Digital APM system. Limited-resolution view mode supports limited access to overview pages and data collection. Resolution view mode is determined by the type of device that is used to access GE Digital APM, and is not a selectable option.
Note: Interaction with diagramming and design canvases is not available on touch-screen devices. If needed, use a mouse peripheral to utilize this functionality.
Minimum Requirements | Devices Tested |
---|---|
Minimum requirements for full-resolution view mode:
|
Devices used in the GE Digital testing environment:
|
Minimum requirements for limited-resolution view mode:
|
Devices used in the GE Digital testing environment:
|
Note: You can access only the Rounds Data Collection module in portrait mode on small screen devices.
Minimum Requirements | Devices Tested |
---|---|
Minimum requirements:
|
Devices used in the GE Digital testing environment:
|
Software Requirements
The following software components are required on any machine or device that will access the GE Digital APM system.
One of the following browsers is required for desktops, laptops, and mobile devices:
Chrome 43 or higher
Note: If your system uses Data Guardian from Koingo Software and you use the Google Chrome browser, you may have to use the browser in Incognito mode to successfully access GE Digital APM.
Safari 8 (Mac only)
Note: You can access GE Digital APM via the browser on a mobile device, but it is recommended that you install and use the GE Digital APM mobile application for an enhanced experience. On a mobile device, to ensure that the mobile application works as intended, you should set your default browser to the desktop versions of Chrome or Internet Explorer (as opposed to the application versions).
One of the following operating systems is required for desktops and laptops:
One of the following operating systems is required for mobile devices:
Copyright © 2018 General Electric Company. All rights reserved.