Create Recommendation Nodes in Policy Designer

A Create Recommendation node represents an action to create a Policy Recommendation record that is populated with the input values that you specify on the Properties window for the node and includes (in the Recommendation Description field) a summary of the policy logic that caused the record to be created.

The outputs of the Create Recommendation node are the following system fields for the record that the node creates: Content GUID, Entity KeyThe Entity Key output can be used in subsequent action nodes, such as the Create Relationship node, but will return a value of 0 if used in a calculation or a Return Value node, since the Entity Key is not available until the record is saved at the end of policy execution., Entity ID, and Site Key.

HintClick here to see an example of this node used within a complete policy model.

Copyright © 2018 General Electric Company. All rights reserved.