Create Entity Nodes in Policy Designer

A Create Entity node represents an action to create new records in any baseline or custom entity family. The fields in the new records are populated with the input values that you specify on the Properties window for the node.

The outputs of the Create Entity node are the following system fields for the records that the node creates: collectionA set of results from a Query node or a set of readings associated with input nodes such as Measurement Location, Health Indicator, or OPC Tag., Content GUID, and Entity KeyThe Entity Key output can be used in subsequent action nodes, such as the Create Relationship node, but will return a value of 0 if used in a calculation or a Return Value node, since the Entity Key is not available until the record is saved at the end of policy execution..

HintClick here to see an example of this node used within a complete policy model.

Copyright © 2018 General Electric Company. All rights reserved.