System Code Tables Used by MOC

The following table lists the System Code Tables that are used by MOC.

Table ID

Table Description

Function

MI MOC ANS OPT MOC Answer Options

Populates the Answer field in MI MOC Answer Option records. By default, this table contains the following values:

  • Yes
  • No
  • NA

A user with administrator privileges can modify this table to include additional answer options.

MI EXCEPTIONS STATE Exception States

Populates the Status field in the MI MOC Exception records. By default, this table contains the following values:

  • Not Started
  • In Progress
  • Complete
MI Change Project Duration Change Project Duration Type

Populates the Change Duration field in the MI MOC Change Project records. By default, this table contains the following values:

  • Permanent
  • Temporary
MI Change Project Type Change Project Type

Populates the Change Type field in the MI MOC Change Project records. By default, this table contains the following values:

  • Temporary
  • Permanent
  • Minor Instrument Change
  • Personnel

A user with administrator privileges can modify this table to include additional change types.

Copyright © 2018 General Electric Company. All rights reserved.