MI MOC Change Project records store information about the Change Project. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Change Project family and appear on the MI MOC Change Project datasheet. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Change Duration | Character | Indicates whether the change is a permanent change or a temporary change. |
This field appears as a list that is populated by the MI_Change_Project_Duration System Code Table. |
Change Project ID | Character | The identification for the Change Project. |
This field is required. You must enter a unique value in this field. |
Change Type | Character | Indicates the type of change managed by the Change Project. |
This field appears as a list that is populated by the MI_Change_Project_Type System Code Table. |
Change Valid Until | Date | The date up to when the change is valid. |
This field is enabled only if the value in the Change Duration field is Temporary. You can select a date in this field. |
Description | Character | A description for the Change Project. | You can enter a value manually. |
End Date | Date | Indicates the date when the Change Project was completed. | You can select a date in this field. The date that you select in this field must be later than the date specified in the Start Date field. |
Owner | Character | The name of the team member who is responsible for managing the Change Project. |
You can enter a value manually. |
Purpose | Character |
A description of the goal of the Change Project. |
You can enter a value manually. |
Scope | Character | A description of the intended scope of change to be accomplished through the Change Project. | You can enter a value manually. |
Start Date | Date | Indicates the date when the Change Project was started. | By default, this field contains the date on which the Change Project was created. You can modify the date. |
Copyright © 2018 General Electric Company. All rights reserved.