MI MOC Answer Option records store information about an Answer Option for a Question and the corresponding Exception that must be created for the Answer Option. When MI MOC Checklist Question records are created by copying the Checklist Question records that you created in the Application Settings for MOC for the Checklist, the associated Answer Option records are also copied. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Answer Option family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Answer | Character | Identifies the response that triggers an Exception. |
This field is populated with the value in the Answer field of the MI MOC Answer Option record whose copy is being created. |
Exception ID | Character | The identification of the Exception that will be triggered on selection of the response indicated in the Answer field. |
This field is populated with the value in the Exception ID field of the MI MOC Answer Option record whose copy is being created. |
Exception Key | Numeric | The Entity Key of the Exception indicated in the Exception ID field. |
This field is populated with the value in the Exception Key field of the MI MOC Answer Option record whose copy is being created. This field does not appear on the datasheet. |
Is Admin Setting | Boolean | Indicates whether the Answer Option represents a record created in the Application Setting. |
This field does not appear on the datasheet. This field is True if you created the record using the Application Settings for MOC. This field is False if GE Digital APM automatically created the record as a copy of the Answer Option that you created. |
Copyright © 2018 General Electric Company. All rights reserved.