RBI 581 Inspection Auto-Selection Workflow

This workflow provides the basic, high-level steps for the Inspection Auto-Selection feature. The steps and links in this workflow do not necessarily reference every possible procedure. For more procedures, see the links in the Related Information section.

  1. Access the Inspection Auto-Selection workspace.
  2. In the upper-right corner of the workspace, select the Inspection Auto-Selection check box.
  3. Review the baseline RBI Inspection Auto-Selection Criteria records.
  4. In RBI, create an RBI Component, and link it to Potential Degradation Mechanisms (PDMs).
  5. Create an RBI 581 Risk Analysis.

    Inspections are automatically assigned to the DMEs based on the criteria in the RBI Inspection Auto-Selection Criteria record.

  6. Review the Inspections assigned automatically to the DMEs.

    For RBI 581 Thinning and Lining Evaluation (only if evaluating 581-Atmospheric Tank Bottom Corrosion), RBI 581 Cracking Damage Evaluation, and RBI 581 External Cracking Damage Evaluation, the following fields are populated automatically:

    For RBI 581 Thinning and Lining Evaluation (if evaluating a Damage Mechanism (DM) other than 581-Atmospheric Tank Bottom Corrosion) and RBI 581 External Damage Evaluation, the following fields are populated automatically:

Copyright © 2018 General Electric Company. All rights reserved.