RBI Inspection Auto-Selection Criteria Records

RBI Inspection Auto-Selection Criteria records store details about the criteria that must be used to assign Inspections automatically to a Damage Mechanism Evaluation (DME). This topic provides an alphabetical list and description of the fields that exist for the RBI Inspection Auto-Selection Criteria family. The information in the table reflects the baseline state and behavior of these fields.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

Analysis Family Character The type of the analysis for which Inspections must be automatically assigned to the DME. The value in this field is RBI 581 Risk Analysis. You cannot modify this value.
Degradation Mechanism Character The DM that is related to the analysis.

If you create, duplicate, or apply an RBI 581 Risk Analysis, and if the analysis is linked to the DM specified in this field, then Inspections linked to the same DM are automatically assigned to the DME based on the criteria in this record.

If this field is blank, all the DMs related to the DME specified in the DM Methodology and Equivalent DM Methodology are considered while assigning Inspections to the DME.

DM Methodology Character The Degradation Mechanism Evaluation (DME) record to which the DM belongs.

Inspections that must be assigned to a DME are filtered based on the values in the DM Methodology and Equivalent DM Methodology fields.

Equivalent DM Methodology Character The equivalent (or related) DME that is associated with the DME specified in the DM Methodology field.

This field is disabled and populated based on the value in the DM Methodology field as follows:

DM Methodology Equivalent DM Methodology
RBI 581 Cracking Damage Evaluation Criticality Env. Crack. Deg. Mech. Eval.
RBI 581 External Cracking Damage Evaluation N/A
RBI 581 External Damage Evaluation Criticality Ext. Corr. Deg. Mech. Eval.
RBI 581 Thinning and Lining Evaluation Criticality Int. Corr. Deg. Mech. Eval.
Years of Inspection History Numeric The duration, in years, that should be considered while assigning Inspections to a DME. If an Inspection is completed before the duration specified in this field, it is not assigned to the DME.

If the difference between the date on which the analysis is created and the value in the Completion Date field in an Inspection is greater than the value in this field, then the Inspection is not assigned to the DME.

Copyright © 2018 General Electric Company. All rights reserved.