The following table outlines the steps that you must complete to deploy and configure this module for the first time.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Important: If you are using SSL, make sure you have configured SSL correctly.
Step | Task | Notes |
---|---|---|
1 | Deploy the APM Connect Base. | This step is required. |
2 | On your APM Connect server and on your GE Digital APM Application Sever, set permissions for the APM Connect Directory. | This step is required. |
3 | On your APM Connect server, deploy and configure data loaders files. | This step is required. |
4 | On your APM Connect server, deploy and configure the APM_UPDATE_LOGIC Webservice. | This step is required. |
5 | In the APM Connect Administration Center, create the Intermediate Repository database. | This step is required. |
Copyright © 2018 General Electric Company. All rights reserved.