Before you begin importing data into GE Digital APM using the Excel source files, you must set up a network folder share. The data is passed from the APM Server to the APM Connect server through a file share, a situation in which a folder on the network is shared and accessible to both servers. This topic describes the steps for setting up the permissions required to enable the file share.
Steps:
To create a domain user for the APM Container:
In the Search programs and files box, search for Run.
Run appears in the Programs list.
Open Run.
The Run window appears.
In the Open box, enter: services.msc.
Select OK.
The Services window appears.
Right-click APM-CONTAINER, and then select Properties.
The APM-CONTAINER Properties window appears.
Enter the credentials for a user within your network, designated to run APM Connect services.
Example: user1@meridium.com
Select Apply, and then select OK.
A domain user has been assigned to run the APM Container service and the Tomcat service.
To create a Data Loaders file share:
IMPORTANT: If you are employing a load-balancing setup using multiple servers, before you proceed, you must first configure the APM Server file share. If you are employing a standalone server, you may proceed with the following steps.
In the directory window, select New folder, and then name the folder with the recommended name: DataLoaderFiles.
The Data Loader files folder is created.
Point to Share with, and then select Specific people....
The File Sharing window appears.
In the Permission Level column for that user, select the drop-down arrow, and then select Read/Write.
Note: Users running the APM-CONTAINER service and the APM Server must have Read/Write access to this folder.
Select Share.
Permission for the folder is granted to the user that you selected.
Grant Read/Write Access to the APMConnect folder:
If you installed APM Connect in the default location the folder is C:/APMConnect.
Right-click on the folder APMConnect, and then select Properties.
The APMConnet Properties window appears.
Select the Security tab, and then select Edit.
The Permissions for APMConnect window appears.
Select Add....
The Select Users, Computers, Service Accounts, or Groups window appears.
Select Check Names.
The APMConnect user's name is validated.
Select OK.
The Select Users, Computers, Service Accounts, or Groups window closes, and the APM Connect user is populated in the Group or user names box.
Select OK.
The Permissions for APM Connect window closes.
On the APMConnect Properties window, select OK.
The APM Connect service user has access to the APM Connect folder.
What's Next?
Copyright © 2018 General Electric Company. All rights reserved.