Note: The APM Connect installer automatically deletes the file RunDataLoaderRoute.cfg from the following location C:\APMConnect\Utilities\runtime\deploy, if it exists there. You must complete the remaining steps in this topic manually.
Steps
Open the file to edit, and then configure the following parameters:
Parameter | Description | Default or Recommended Value |
---|---|---|
context | Defines what Talend context environment is used. | Default. |
TRUSTSTORE_FILE | The directory path to the dinoloader SSL configuration file. | Value is unique to the user. |
TRUSTSTORE_PASSWORD |
The password for the keystore files. |
Value is unique to the user. |
USE_SSL | Determines if SSL is used. |
|
IR_HOST | Intermediary Repository host name. | Value is unique to the user. |
IR_DATABASE | Database for the dinoloader job. | Value is unique to the user. |
IR_USERID | Intermediary Repository username. | Value is unique to the user. |
IR_PASSWORD | Intermediary Repository password. | Value is unique to the user. |
IR_SCHEMA |
The schema in which the IR database will be created. |
The default value is public. |
IR_PORT | Intermediate Repository port. | Default value is 5432. |
LOG4J_CONFIG_FILE | Log4j directory path. | C:/APMConnect/Config/log4j.properties |
IS_LINUX | Indicates if the machine on which the Data Loaders are deployed is a POSIX-compliant operating system (e.g., Linux, UNIX, AIX, HPUX etc.) or another operating system. |
|
LINUX_BASE_PATH | The directory path where the data loader file share is mounted. |
This parameter is required only if you are deploying the Data Loaders on a Linux machine. This path is defined by system administrator for the Linux machine, and the value is unique to the user. |
ROW_LEVEL_LOGGING | Used for debugging, specifies whether or not data rows are written to the log. |
The default is false. true: Writes data rows to the log. false: Suppresses data rows from the log. |
org.apache.karaf.features.configKey | Karaf web console configuration tie-in is used to associate this configuration file with the RunDataLoaderRoute class. |
RunDataLoaderRoute.talendcontext.Default IMPORTANT: Do not modify this parameter. |
On your APM Connect server, navigate to <root>\APMConnect\Utilities\runtime\deploy, and then paste the copied file in that location.
Note: If new configuration is not automatically applied, restart the APM_CONTAINER service. This will force the changes to be applied.
What's Next?
Copyright © 2018 General Electric Company. All rights reserved.