Activate and Maintain your GE Vernova Manufacturing Licenses
The following are the different options to activate your GE Vernova product licenses:
Activate and maintain licenses by connecting clients to Cloud License Server
When to choose this option: This is the simplest way to activate Proficy software product licenses in your online computer (physical machine) and is recommended unless central management or support for virtual machines are required.
Use this option when the computer (physical machine or virtual machine) with Cloud License Server is connected to internet.
How it works: You must connect to Cloud License Server to activate your licenses on the client computer. This is a one-time connection. Options for both online and offline license clients are available. The License Client does not need to stay connected to the Cloud License Server; you only need to connect again if you choose to Return or Refresh your activation from the License Client.
Refer to: Activating Licenses on a Computer Connected to the Cloud License Server to activate licenses on a computer connected to the Cloud License Server.
Activate and maintain licenses on a Local License Server
When to choose this option: Local license servers enable you to manage and distribute licenses from a central machine on your network. They are also required if you are running your licensed GE Vernova applications on virtual machines. You can host the license server on the same computer.
You must use this option when the computer (physical machine or virtual machine) with Local License Server is connected to internet.
How it works: You will install the GE Vernova Common Licensing software on a local machine, then make a one-time connection to the Cloud License Server to load licenses onto your Local License Server. Client computers then connect to the Local License Server and lease their licenses. License Clients must remain connected to the Local License Server to renew their leased licenses every few hours. If a License Client is unable to connect, you will receive the warning message: This License is about to expire. After 21 days (this limit is configurable) of activating GE Vernova licenses, the License Client will lose its activation lease, you cannot run the licensed application(s) and the activation will automatically be returned to the Local License Server.
Refer to: Activating Licenses on a Computer Connected to a Local License Server to activate Licenses on a computer connected to a Local License Server.
Activate and maintain licenses using a USB Hardware key
When to choose this option: Use this option when your physical or virtual computers are not connected to internet or intranet. Also, if the license key is tied to a USB device (so it is easy to ship to remote locations or move between the devices).
- Non-configurable USB Hardware keys are pre-loaded with the licensing information for your products. You cannot modify the licensing information contained in these keys. However, if you need additional licenses, you can purchase them from GE Vernova and then re-flash keys with an image file (supplied by GE Vernova) that overwrites all existing information and replaces it with updated licensing information.
- Configurable USB Hardware keys are plugged into a computer connected to the
internet to activate licenses on the USB stick from the Cloud License Server. Note:The USB Hardware keys cannot be activated from a Local License Server. Any license changes, upgrades, or returns require the hardware key to be plugged into a computer connected to the internet, and to ensure that the Cloud License Server can be accessed.
Refer to: Activating Licenses on a Computer with a USB Hardware Key Inserted to activate Licenses on a computer connected to USB Hardware key.
Licensing Methods Comparison Table
The following table provides a quick comparison of the licensing methods as described above:
Cloud License Server | Local License Server | Non-Configurable USB Hardware key | Configurable USB Hardware key | |
---|---|---|---|---|
Client type | Physical Machine | Physical Machine or VM | Physical Machine or VM | Physical Machine or VM |
Network access |
|
|
None | One-time client access to internet for activation, changes, updates, or return. |
Number of clients | Unlimited | <100 clients per server | Each USB Hardware key may only have up to one copy of each GE Vernova Manufacturing product. | |
Additional considerations | This option does not provide centralized license management for multiple clients. |
|
Changes, updates, or additional licenses require USB to be re-flashed using an image file provided by GE Vernova. | USB Hardware keys cannot be activated from a Local License Server. |