Create Picture Wizard Dialog Box

Common Wizard Elements

The Create Picture Wizard guides you when creating pictures in Configure mode that will appear the way you intend in Run mode. Each page in the Wizard includes the following elements:

  • Preview Pane – Shows a picture configuration based on the currently selected options.
  • Help Button – Launches the Help topics for the Create Picture Wizard.
  • Cancel Button – Exits the Create Picture Wizard without creating any new pictures, and without changing WorkSpace appearance.
  • Previous Button – Returns you to the previous page in the Wizard.
  • Next Button – Sends you to the following page in the Wizard.
  • Finish Button – Creates the new pictures that you have specified, and sets the WorkSpace appearance that you have specified. This button is only enabled when the Wizard has collected enough information to successfully create new pictures.

Create Picture Paths

The Create Picture Wizard dialog box displays three paths to create new pictures. For more information on the screens that appear when you select a path, refer the following sections:

Show WorkSpace Appearance Page

Indicates whether you want to view the WorkSpace Appearance page in the wizard. This page only needs to be accessed once per WorkSpace session.

Do not show this Wizard from the new picture menu and Exit now

Prevents the wizard from running the next time you select New Picture from the File menu. The Finish Button changes to an OK button, and allows you to close the wizard.

How Do I...