To define the
attributes of a custom picture:
- In the iFIX WorkSpace, run the Create Picture Wizard and create a custom picture.
- Proceed through the wizard until you reach the Define Custom Picture Attributes page.
- Select or clear the check boxes for the following attributes:
- Show Title Bar – Adds a title bar to your picture.
- Show System Menu – Adds system menus to your picture.
- Resizable – Adds sizing borders to the picture.
- Always on Top – Configures the window so that it is always on top when you open it.
- Allow this picture to be cached – Configures the window so that when it is opened and closed it is held in memory and, when reopened, is read from memory.
- Click the Background Color button to set the actual background color of the picture. This color appears in the preview pane.
See Also