To access the
Create Picture Wizard:
Use any of the following methods in the iFIX WorkSpace to access the Create Picture Wizard:
- Menu Bar – On the File menu, point to New and then click Picture (Classic View only).
- Ribbon – Click the WorkSpace button, select New, and then click Picture (Ribbon View only).
- System Tree – Right-click the Pictures folder in the System tree and select New from the pop-up menu.
- Task Wizard – Click the Task Wizard button on the Standard toolbar, select Picture from the Task Categories list box, then select Create Picture Wizard from the Tasks list.
- Experts Toolbar – Click the Create Picture Wizard button on the Experts toolbar.
- Standard Toolbar – Click the New Picture button on the Standard toolbar.
- Toolbox – Click the Create Picture Wizard button on the Toolbox.
NOTE: To access the Create Picture Wizard from the Menu Bar, the Ribbon, the System Tree, or the Standard toolbar, you must have the Show Picture Wizard from New Picture Menu check box enabled on the Picture Preferences tab of the User Preferences dialog box.
See Also