Understanding Security Synchronizer Messages

You may encounter the errors listed in this section in the iFIX alarm destinations or the iFIX security log file while Security Synchronizer is running. Error codes can range from 0, indicating that no errors have been detected, to 299.

The error code associated with a specific error is written to the analog error tag, if a valid tag is specified with the /E parameter. If more than one error occurs during the security synchronization process, then the most severe error code is written to the analog tag. If more than one error of the same severity is encountered, then the last error generated of that severity is written to the analog tag.

If an error is encountered while the security synchronization is processing, then the digital error tag is set to 1.

Error messages that contain user names display the Windows user name in the message. Refer to the following sections for more information about error messages:

 

See Also