Command Line Parameter Errors

Values are not associated with command line parameter errors since values are not written to the iFIX database when these errors occur. These errors terminate the synchronization process before it actually begins. These errors are detected only when the SecuritySynchronizer.exe program is running, and not when programming to the Security Synchronizer Automation interface. Refer to the iFIX Automation Interfaces Help file for more information on the Automation interface.

You may encounter one of these command line errors while running Security Synchronizer:

  • Security Synchronizer: Invalid Windows Domain name. Synchronization aborted.
  • Security Synchronizer: Invalid Login Timeout value. Value must be between 0 and 86399 seconds. Synchronization aborted.
  • Security Synchronizer: Invalid MapMode value. Synchronization aborted. FOR FUTURE USE.
  • Security Synchronizer: Invalid Analog Error Tag syntax (/E). Synchronization aborted.
  • Security Synchronizer: Invalid Failure Tag syntax (/F). Synchronization aborted.
  • Security Synchronizer: Invalid Completion Tag syntax (/C). Synchronization aborted.