Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Select the Accept check box to accept the license agreement, and select Next.
If needed, change the installation drive, and then select Next.
If needed, change the port number for the NodeJS server to run. This step is required if the default port number is not available.
Select Next.
Select Install.
The Help is installed.
Select Next.
Results
The Help is installed. You can access the Help from any of the Historian applications or by accessing the index.html file. By default, this file is available in the C:\Program Files (x86)\GE Digital\Historian Help folder.