After you have installed the Historian server and restarted your system, you can install additional components, such as Client Tools, the Historian Excel add-in, the Web-based Clients, data collectors, and Historian Alarms and Events.
Historian Administrator
and the
OPC Classic HDA
server are installed as part of the
Client Tools installation.
Note: On a 64-bit Windows operating system, the default
destination folder for all 32-bit components (such as collectors and
APIs) is C:\Program Files\Historian\x86.
Similarly, for all 64-bit components (such as Excel Add-in 64-bit
and SQL Server 64-bit), the default destination folder is
C:\Program
Files\Historian\x64.