Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
Install the Historian Excel Add-in at a Command Prompt
Before you begin
Install one of the following 32-bit or 64-bit Microsoft® Excel® applications:
Microsoft® Excel® 2019
Microsoft® Excel® 2016
Microsoft® Excel® 2013
Microsoft® Excel® 2010
Install Excel Add-in using
the installer on a machine. When you do so, a template file named
setup.iss is created at
C:\Windows. This file stores the installation options that
you have provided during the installation. You can then use this template to
install Excel Add-in at a command prompt on other machines.
About this task
You can install Excel Add-In separately or during Client Tools installation. However, do not install Excel Add-In on the machine on which you have
installed Historian Administrator or data archiver.
Procedure
Copy the setup.iss file to each machine on which you want
to install Excel Add-in at a command prompt.
In the folder that contains the setup.iss file, run the
following command: setup.exe /s /sms
The installer runs through the installation steps.
Note: If using certain
versions of Windows (like Windows 10 or Windows 2019), you may receive an
error message, stating that some of the DLL files are not registered. You
can ignore these messages.