Install Client Tools at a Command Prompt
Before you begin
- If you want to install Excel Add-In for Historian, install one of the following
32-bit or 64-bit Microsoft® Excel® applications:
- Microsoft® Excel® 2019
- Microsoft® Excel® 2016
- Microsoft® Excel® 2013
- Microsoft® Excel® 2010
- Install Client Tools using the installer on a machine. When you do so, a template file named setup.iss is created at C:\Windows. This file stores the installation options that you have provided. You can then use this template to install Client Tools at a command prompt on other machines.
About this task
- Client Tools
- Historian Administrator
- OLE DB driver and samples
- The OPC Classic HDA server
- User API and SDK
- Historian Client Access API
- Collector Toolkit