Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
Create a UAA Reader Client Using the UAA Config Tool
About this task
To fetch Historian data, previously, you had to manually add each user to iH
security groups. Only then the users could fetch the data. Now, this process has been
simplified. All you must do is create a UAA client. The UAA client will be automatically
added to the iH Readers security group on the server side. Therefore, you can use the
client to fetch Historian data using REST APIs.
Procedure
Access the UAA Config tool, which is located in the following folder y default:
C:\Program files\GE Digital\Historian Config
Access Command Prompt as an administrator, and then run the following
command: