Release Notes
Historian Release Notes
Description | Tracking ID |
---|---|
Sending Collector Data to Alibaba Cloud In addition to Google Cloud, AWS Cloud, and Azure Cloud, you can now send collector data to Alibaba Cloud via MQTT using Configuration Hub as well as the RemoteCollectorConfigurator utility. |
F60805 |
Installing Operations Hub and Historian Web-based Clients on the Same Machine You can now install Operations Hub and Web-based Clients on the
same machine. To facilitate this enhancement, after you install
Operations Hub, if you install Web-based Clients on the same
machine, the FQDN is disabled and populated with the value you
provided while installing Operations Hub (and vice versa).
Note: When Tomcat is restarted, the CPU utilization
increases for some time. Therefore, we suggest that you
restart only one instance of Tomcat at a time. |
F59167 |
Access to Cross-Domain Historian Systems You can now access Historian across various domains regardless of the domain to which your user account belongs. For instructions on providing cross-domain Historian access, refer to About Accessing Cross-Domain Historian . |
F59177 |
UAA Reader Client Creation Using the UAA Config Tool To fetch Historian data, previously, you had to manually add each user to iH security groups. Only then the users could fetch the data. Now, this process has been simplified. All you must do is create a UAA client. The UAA client will be automatically added to the iH Readers security group on the server side. You can then use the client to fetch Historian data using REST APIs. For instructions, refer to Create a UAA Reader Client Using the UAA Config Tool. |
|
Licensing Enhancements for a Distributed Environment To set up a distributed/mirror environment, previously, the
Enterprise license was used, which you could apply for one
primary and two distributed/mirror servers. Now, the licensing
is separate for primary and distributed/mirror servers:
|
F60333 |
Automatic Creation of Collector Instances When you install collectors, if iFIX and/or CIMPLICITY are
installed on the same machine as the collectors, instances of
the following collectors are created automatically:
When you uninstall collectors, these instances of collectors (the ones that are created during the installation of collectors) are deleted automatically. |
|
New Utility to Update UAA Server Details If you have changed the UAA server used by Web-based Clients, you can now update the UAA server details for the Historian server without the need to reinstall it. The Historian server and Web-based Clients will then point to the same UAA server, which is required for you to access Web-based Clients (such as Configuration Hub, Trend Client, the Web Admin console, and REST APIs). To facilitate this enhancement, the UAA Configuration tool has been introduced. Using this tool, you can provide the UAA server details that you have provided during the installation of Web-based Clients. For instructions on using this tool, refer to Change the UAA Server. |
US494635 |
Description | Tracking ID |
---|---|
Previously, an error occurred during the installation of Client Tools and Excel Add-In for Historian 8.1 because the DLLs were not registered correctly. This issue has been resolved. | DE138680, DE146006 |
Previously, you could not set up Historian in a clustered environment because loading the Historian DLLs failed. This issue has been resolved. | DE162167 |
Previously, there was a discrepancy between the alarms logged in iFIX and the Historian Alarms and Events database. This issue has been resolved. | DE161609 |
Previously, several mdmp files were created in C:\Program Files\GE\Historian\historian-tomcat. This issue has been resolved. | DE161705 |
Previously, when you attempted to fetch a list of OPC servers
using the Get OPC Server API, an error occurred. This was applicable
to the following OPC servers:
|
DE147276 |
Previously, if you upgraded collectors, you could not manage the OPC collectors. An error message appeared in the CollectorManager.shw file. This issue has been resolved. | DE151366 |
Previously, after you upgraded Historian, the File Collector service was not available. This issue has been resolved. | DE156501 |
Previously, if you upgraded Historian from a version earlier than 8.1, by default, storing future data was enabled. This issue has been resolved. | DE149376 |
Previously, when you attempted to use the Client Access API, a DataParc List Tags error occurred. This issue has been resolved now. | DE153966 |
Previously, after you purged and restored alarms data, the restored data did not match the original data. This issue has been resolved. | DE109010 |
Previously, when you fetched alarms data, duplicate alarm comments appeared. This issue has been resolved. | DE120509 |
Previously, when you queried for interpolated data using the Excel Add-In, the expected result was not returned. This issue has been resolved. | DE140629 |
Previously, the OPC Classic DA collector crashed if a tag of the float or integer data type was configured as a variable string. This issue has been resolved. | DE158901 |
Description |
---|
You can install Configuration Hub only in the C
drive. Workaround:
|
If an iFIX collector instance created in version 9.0 exists, after you upgrade collectors, another instance of the iFIX collector is created. Because of this, the Remote Collector Manager (RCM) will not work correctly. Therefore, if you want to use RCM, you must delete one of the instances. If needed, you can manually create another instance of the iFIX collector using Configuration Hub or the RemoteCollectorConfigurator utility. This is applicable to the iFIX Alarms and Events collector as well. |
If the Configuration Manager service is down, you cannot query
tags and data in a horizontally scalable system. However, you can
query tags and data in the following scenarios:
|
You cannot change the destination of a collector instance from Historian to Predix TimeSeries. Create a new instance as required. |
Using Configuration Hub, you cannot add comments, pause data collection, resume data collection, or modify an instance of offline collectors. In addition, you cannot compress network messages. You can, however, enable the debug mode and delete the collector instance. |
Configuration Hub is not supported in a clustered Historian environment. |
If you have logged in to Operations Hub, and then if you try to
access Web-based Clients, and vice versa, an error occurs. This is
because the user credentials of the first application to which you
have logged in are used to log in to the other one as
well. Workaround: Try one of the following
options:
|
Description | Tracking ID |
---|---|
During Web-based Clients installation, if you provide an external
UAA and Configuration Hub, and if the public https port numbers of
these two machines do not match, you cannot access the external
Configuration Hub from the current machine. For example, suppose you have installed Web-based Clients on machine A, which points to the UAA and Configuration Hub installed on machine B. If the public https port numbers of machines A and B do not match, you cannot access Configuration Hub of machine B from machine A (although you can access it locally from machine B). Workaround: Perform the following steps on
the machine on which you have installed Configuration Hub
(machine B):
|
DE162153 |
If you install Configuration Hub using iFIX, then install
Web-based Clients on another machine with local UAA, and then
register the Historian plugin with Configuration Hub, testing the
connection to Configuration Hub fails. Even after you add the IP
addresses of both the machines to the hosts file, the issue is not
resolved. Workaround: Register the Historian plugin on the machine on which you have installed Web-based Clients, install the UAA certificate, and then restart the browser. |
DE161847 |
If a tag name contains the following special characters, you
cannot retrieve the tag data using REST APIs, the Web Admin console,
or Trend Client:
|
DE160889 |
If you install only Client Tools, the SDK sample is not downloaded. | DE161595 |
When you upgrade to Historian 9.1, after installing Web-based
Clients, a message asking you to restart the machine does not
appear. Because of this, sometimes, you cannot access Web-based
Components such as Configuration Hub, Trend Client, the Web Admin
console, and REST APIs. Workaround: Restart the machine, or
start the following services:
|
DE160543 |
If you upgrade the Server-to-Server collector from 8.1, you
cannot send data to Azure IoT Hub using that collector instance.
This is because the syntax of the connection string has changed. You
can, however, send data by adding another collector instance. For information on the connection string syntax, refer to Collector Instance Parameters. |
DE157795 |
You cannot set up Historian in a cluster environment using Historian.dll. | DE159583 |
For a collector instance whose destination is Azure IoT Hub, you
cannot restart the collector using the Save and
Restart button in Configuration Hub. You cannot
restart the collector using the Windows service
either. Workaround: Use the Restart Collector API to restart the collector. |
DE151454 |
After you delete a collector instance, the Windows service and
the registry entry for the collector are not
deleted. Workaround: Delete the Windows service and the registry entry manually. |
DE151169 |
If the version of Historian collectors is different from that of
Client Tools, ihSQL does not work. Workaround: Ensure that you have the same version of Client Tools and collectors. |
DE149550 |
Using Configuration Hub, if you add a system by specifying its host name, and then add the same system by specifying its IP address, or vice versa, no validation error appears. | DE146366 |
When Configuration Manager is down, you cannot browse for tags in a horizontally scalable system. | DE141885 |
If you register the Configuration Hub plugin with a remote
Configuration Hub container, the local instance of the connection is
not unregistered. Workaround:
|
DE150907 |
If you install Configuration Hub and the Web Admin console on the
same machine, and use self-signed certificates for both of them, the
login page for Configuration Hub does not appear.
Workaround: Disable the domain security
policies:
|
DE151105 |
You cannot create multiple instances of the File collector on a single machine. | DE151715 |
Using Configuration Hub, you cannot restart an OPC collector
whose destination is Azure IoT Hub. Workaround: Restart the collector from the Collectors section in Configuration Hub, modify the registry entry for the collector instance and restart manually, or restart the collector machine. |
DE151454 |
When you change the destination of a collector from Historian to Predix TimeSeries, no success message appears although the destination is changed. In addition, the collector is not started automatically. | DE151859 |
Even after you uninstall collectors and Web-based Clients, the corresponding Windows services and registry entries are not removed. | DE151169 |
When you upgrade iFIX collectors to version 9.0, the custom registry folders are deleted. | DE151435 |
In Configuration Hub, for a stand-alone Historian system, when you select a server, the Diagnostics Manager service does not appear in the Details section. | DE151711 |
If you upgrade Historian server from a single-server installation
to a primary mirror installation, and if you then add a distributed
machine to the Historian system using Configuration Hub, you may see
issues in connecting the distributed machine to the primary
machine. Workaround: Restart all the Historian server services on Primary Mirror server and Distributed/Mirror server machine. |
DE152582 |
In a horizontally scalable system, if Client Manager is down, Web-Based Clients do not failover to the other Client Managers in the system. And, the following error message appears in Web-Based Clients: Service call to central buffer server fail. | DE152830 |
In a horizontally scalable system, instead of adding a distributed machine, if you add a primary mirror machine or a monolithic (stand-alone) machine, no validation message appears, but causes issues later. |
DE153191 |
If you upgrade Historian server to 9.0, the machine is restarted abruptly when the installation is still in progress. The installation will, however, resume after the machine is restarted. | DE151125 |
If you upgrade Historian server from a mirror system to a horizontally scalable system in 9.0, you cannot query data from the distributed machine when the distributed machine is removed from the DefaultMirror location. | DE152677 |
If you install iFIX on a machine that has Historian Web-based
Clients, sometimes, the reverse proxy service stops
working. Workaround: Restart the reverse proxy service - GE Operations Hub Httpd Reverse Proxy. |
DE151157 |
If you reinstall collectors and Web-based Clients, the size of the Historian server and Web-based Clients appears as decreased in the Programs and Features page, although there is no functional impact. | DE152484 |
When you install Client Tools, incorrect installation pages
appear, although the installation is
successful. Workaround: Ignore the incorrect installation pages, and proceed with the installation of Client Tools. |
DE153175 |
If you change the destination of a collector instance, the destination is not updated in the older machine, although the destination is updated in the new machine. | DE153176 |
Even if you install Web-based Clients using an alias name, you cannot access Configuration Hub using the alias name. | DE148939 |
While connecting to a remote Historian, you cannot add an instance of the File collector unless Client Tools are installed. | DE152330 |
In Configuration Hub, for a horizontally scalable system, in the
Collectors section, you cannot access an
offline collector; a blank error message
appears. Workaround: Ensure that the URI registry entry is the same for all the machines in a horizontally scalable system. |
DE151380 |
If you upgrade collectors to version 9.0, an error occurs when
you access Historian Administrator. Workround: Install Client Tools. |
DE151932 |
While installing Web-based Clients, after the connection to the
external UAA is successful, if you change the UAA details, you can
proceed to the next step even without testing the connection.
Because of this, you will not be able to connect to the UAA server
if the UAA details are incorrect (although you can install Web-based
Clients). Workaround: Test the connection to the external UAA again, and only after the connection is successful, proceed to the next step. |
DE155570 |
You cannot browse for tags in the Server-to-Server and Server-to-Distributor collectors if Windows security is enabled. | DE135459 |
The OPC UA DA collector stops working for unsolicited tags after you disconnect and reconnect to the source. | DE135433 |
In Trend Client, if you have used a calculated data query, and have provided an interval for the data, the query results appear only for half of the interval that you have selected. | DE134193 |
If you attempt to log in to the web admin console as user belonging to the ihsecurity group, and if you use LDAP, an error occurs. | DE134898 |
Archive backup is not functional in the web
admin. Workaround: Perform archive backup using the ihArchiverBackup tool or thick client. |
DE124038 |
File, Calculation, and Simulator collector services are removed
after installing the Client tools. Workaround: Reinstall the collectors after installing the Client tools. |
DE123472 |
When you use Excel Add-in Client tools for Mirror Node the Data Archiver Services are not appearing in services. | DE123374 |
Collectors services are deleted after server is
uninstalled. Workaround: Reinstall the collectors after installing the Client tools. |
DE123370 |
When you install Alarms and Events, Excel Add-In is
uninstalled. Workaround: Reinstall Excel Add-In after installing Alarms and Events. |
DE123292 |
You cannot export only one tag using Excel
Add-In. Workaround: Enter ? after the tag name that you want to export. |
DE123255 |
When Collector Compression is enabled and set to Absolute, the Compression Timeout Value is not retained. | DE123116 |
When compression in turned on with compression timeout, invalid data points are logged. | DE123049 |
The Max. Recovery Time property cannot be for Server-to-Server Distributor. | DE122998 |
The Tags to Recalculate section is disabled in the Recalculate window of the Server-to-Server Distributor. | DE122986 |
When you uninstall collectors, the OPC Collector shortcut is not removed. | DE122882 |
The second data point is not available after data collection is disabled and enabled at source in the Server-to-Server collector. | DE122660 |
AdoptOpenJDK is installed in only C drive even if you choose to install Historian in any other drive. | DE112542 |
Uninstalling Historian 7.1 SIM1 fails on some of the
machines. Workaround: Stop all Historian Server services and then uninstall Historian 7.1 SIM 1. |
DE114135 |
Tags that are associated with ENUM are not correctly displayed in the destination machine when connected using OPC Classic HDA Collector. | DE113677 |
Compression is not applied for OPC Classic HDA cloud collector. | DE114500 |
Prefix is not added to the messages even if message prefix is enabled in the Server-to-Server collector configuration. | DE113857 |
Tag level Security - Administrator group user cannot browse and edit the tag if Read or Write group is already configured. | DE115633 |
If a tag is renamed (not permanent rename - Aliasing), although the tag name is available for selection in the browse tag list (shown in blue color), if you try to select and add the tag, an error message appears. | DE91020 |
In Excel Add-In, the search message functionality does not return expected output when start/end time format is mm/dd/yyyyy HH:mm:ss. | DE93928 |