Installing and Configuring the Collector Toolkit for Linux
Installing and Configuring the Collector Toolkit for Linux
Before you begin
The toolkit is compiled and tested on CentOS 7 and Ubuntu 14. The minimum system requirements are:
- g++(GCC) 4.8.x
- glibc2.17+
About this task
Installing the Collector Tool kit for Linux
The Collector Toolkit is delivered as a tar file. There are four different artifacts to choose from: static and shared library versions of debug and non-debug (release) versions. Choose whichever of the artifacts best fits your needs.Unzip the tar file at a location where you want to install it. There are 4 folders at the top level.
- shared: The shared folder contains an example collector using the Collector Toolkit. A sample Make file is also provided. This example works as is. Your can use this as a template to create your own custom collector.
- lib: The lib folder contains two libraries:
libihAPI
andlibihCollectorDelegator
. - include: The include folder contains include files that you would need to include in your custom collector.
ihAPI.h
is optional. It needs to be included only if you are making use of any System APIs directly in your custom collector. - bin: The bin folder contains some pre-compiled binaries.
Random
is the binary for the Simulation Collector.RandomValueSimulator
is the sample collector built using the example code in the shared folder.