Custom Collector Toolkit Interface Technical Reference
Custom Collector Toolkit Interface Technical Reference
The Collector Toolkit interfaces help in writing collectors with basic functionality such as initializing collectors, adding data and tags, the others help in writing advanced features such as store and forward functions, heartbeat, buffering, queuing. The following are the various interfaces in detail:
ihCollectorToolkitASyncAddTag
The shell will call this function at start up and on change to indicate a tag that should be collected. The collector specific code should keep all information about the tags and use it later to deliver the collected data.
- Prototype
-
int ihInterfaceTKASyncAddTag(ihInterfaceTKASyncTagInfo *ASyncTag, int IsCollectorStarting)
- Returns
- TRUE on success. FALSE if the tag could not be added. For example, if the
tag has an invalid address you can return an error here or report bad data
later after
ihCollectorToolkitAsyncStartReading
is called. - Parameters
-
Name Data Type Description ASyncTag
ihInterfaceTKASyncTagInfo
Refer to the structure description. IsCollectorStarting
int
TRUE if this function is being called as part of collector start-up. FALSE if this is being called because a tag was added or modified while the collector was running.
ihCollectorToolkitASyncDeleteTag
Use this tag to update information to the Collector when a tag is deleted so that it will stop collecting data from the source. For example, if you delete a tag or stop collection in the administrator then the shell will call this function.
- Prototype
-
int ihCollectorToolkitASyncDeleteTag(int tagId)
- Returns
- TRUE on success; your collector specific code should always return TRUE.
- Parameters
-
Name Data Type Description tagId
Int Tag identifier; the tag name is not passed into this function. You would have to match the tag identifier with a magnate passed in ihCollectorToolkitASyncAddTag
.
ihCollectorToolkitASyncInit
The collector shell will call this to indicate the start of a list of tags to be
collected asynchronously. The tags will be delivered via the
ihCollectorToolkitASyncAddTag
function and the collector
specific code should keep track of all tag information.
- Prototype
-
int ihInterfaceTKASyncInit(void);
- Returns
-
TRUE on success; your collector specific code should always return TRUE.
ihCollectorToolkitASyncInitCompleted
The collector shell will call this method to indicate the end of a list of tags to be collected asynchronously.
- Prototype
-
int ihInterfaceTKASyncInitCompleted(void)
- Returns
- TRUE on success; your collector specific code should always return TRUE.
ihCollectorToolkitASyncReload
This function is used to perform a recalculation on all unsolicited tags in the
custom collector. Custom collector must implement the necessary changes to read data
from the source and send values via the
ihCollectorToolkitDataCallback
. The time frame for
recalculation is given in the input parameters StartTime
and
EndTime
.
For more information on the methods of unsolicited tags, refer the methods listed for unsolicited tags in About Interfaces.
- Prototype
-
int ihCollectorToolkitASyncReload(ihTKTimeStruct TimeStruct *StartTime, ihTKTimeStruct TimeStruct *EndTime)
- Returns
- Always, TRUE.
- Parameters
-
Name Data Type Description StartTime
ihTKTimeStruct
Reserved EndTime
ihTKTimeStruct
Reserved
ihCollectorToolkitASyncStartReading
The collector shell will call this method to indicate that the collector should start reading data for asynchronous tags from the source and report any data changes to the shell.
- Prototype
-
int CustomCollector:: ihCollectorToolkitASyncStartReading(void)
- Returns
- TRUE on success; your collector specific code should return TRUE.
ihCollectorToolkitDataCallback
This callback is used when unsolicited tags get the data and asynchronously writes
them into the Historian. Custom collector receives the data from unsolicited tags
and sends it to the ihCollectorToolkitDataCallback
. This call back
function internally writes the data into the Historian.
- Prototype
-
voidihCollectorToolkitDataCallback(void *Param)
- Returns
- Void.
- Parameters
-
Name Data Type Description ASyncTag
ihInterfaceTKASyncData
Refer to the structure description. - Example
- You can use this function as shown in the following example to create a thread using which the unsolicited tags
ihCollectorToolkitDefinitionInitialize
Use this interface to specify what labels you want to appear on the collector configuration page of the administrator. The administrator will show 5 edit boxes for General 1 to General 5 but with this function you can control what text is show next to each edit box.
All custom collectors share the same set of labels.
- Prototype
-
void ihCollectorToolkitDefinitionInitialize(ihCollectorToolkitDefProperties* CustomPropertyDesc)
- Returns
- Void.
- Parameters
-
Name Data Type Description CustomPropertyDesc
ihCollectorToolkitDefProperties
Pointer to a Custom Collector???s specific properties General 1-5 definitions.
ihCollectorToolkitDestroyGroupData
Reserved for future use. Your collector specific code should call the
CCollectorDelegator
function.
- Prototype
-
void ihCollectorToolkitDestroyGroupData(int NumTags, void *Data, void *Misc)
- Returns
- Void.
- Parameters
-
Name Data Type Description NumTags
int
Reserved Data
void
Reserved Misc
void
Reserved
ihCollectorToolkitDebugModeChange
The collector calls this method when a change is detected. 0 indicates only errors and important information should be written to log. 255 is the highest setting for all debug information to display.
- Prototype
void ihCollectorToolkitDebugModeChange(int DoDebug)
- Returns
- Void.
- Parameters
-
Name Data Type Description DoDebug
int
Zero or non zero debug level.
ihCollectorToolkitGetData
This is the function called by the collector shell each time the collector should
poll data from the data source. The shell will pass a list of tags by tag id to be
read. The tagids were provided to the collector specific code in the
PolledAddTag
call. The string tagnames, if needed, are
available in the ihInterfaceTKDataInfo
structure. The collector
should gather the data and fill in the remaining fields of the
ihInterfaceTKDataInfo
.
- Prototype
-
void ihCollectorToolkitGetData(int MinInterval, int AnySourceTimes, int CreatePermGroup, int NumTags, int *TagIds, ihInterfaceTKDataInfo *Data)
- Returns
- Void.
- Parameters
-
Name Data Type Description MinInterval
int
The minimum configured collection interval of the tags being passed in for polling. AnySourceTimes
Int
TRUE if any of the tags to be collected are configured for Time assigned by source. This would mean the collector specific code has to do additional work to provide a timestamp with the data. If this is FALSE, then the collector shell will provide the timestamp. CreatePermGroup
Int
FALSE if this is a one time read such at start up or collector redundancy fail over. In this case, you can choose to not make a permanent collection group inside your code. If this is TRUE, then this is a normal scheduled polled read and you should consider making a permanent group in your code for greater efficiency. NumTags
Int
Number of tags to be read. TagIds
Int
List of tags to be read, identified by tag ID. The tag names are in the data parameter, if required. Data
ihInterfaceTKDataInfo
Pointer to the Proficy Historian Collector Data Properties. This contains some information from the shell and then the collector specific code needs to fill in the collected values. - Example
- Populating data for a single
tag.
ihInterfaceTKDataInfodata; memset(&data,0, sizeof(ihInterfaceTKDataInfo)); data.Tag= L???computername.OperatorName??? data.DataProp.ValueDataType= ihTKFloat; // correct data type- same as tag type data.DataProp.TimeStamp= pColl->TKGetSystemTime(); //10/01/2014 07:05:00 data.DataProp.Value = 10; // value that matches the data type. data.DataProp.Quality = ihTKOPCGood;
ihCollectorToolkitGetTagsHierarchical
Use this interface to retrieve and represent the data in a hierarchical manner.
- Prototype
-
void ihCollectorToolkitGetTagsHierarchical(wchar_t* BrowsePosition, wchar_t* NodeFilter, ihInterfaceTKHierarchicalBrowseResponse* Response)
- Returns
- Void.
- Parameters
-
Name Data Type Description BrowsePosition
wchar_t*
Position of browsing for specific Tag. NodeFilter
wchar_t*
Node filtering required for tag to get hierarchical information.
Response
ihTKHierarchicalBrowseResponse
Hierarchical Groups of tags browse response.
ihCollectorGetTags
Use this interface to browse tags from source. The shell will give some criteria and the collector specific code should fill in the result.
Tags can be skipped when they exist in the data source but should not be collected into Proficy Historian. For example, if a tag has a data type that is not compatible with Proficy Historian, you would not return it and you can increment the number skipped.
- Prototype
-
void ihCollectorToolkitGetTags(ihInterfaceTKTagRecordset *Tags, ihInterfaceTKCfgInfo *Cfg, wchar_t *BrowsePosition, ihTKBoolean Recursive, wchar_t *DescriptionMask, wchar_t *SourceAddressMask, int CanReadASync, int DoMsgPump, int *NumSkipped
- Returns
- Void.
- Parameters
-
Name Data Type Description Tags
ihInterfaceTKRecordset
Pointer to a Proficy Historian Tags Record set containing browse criteria and where you can return the tags. Cfg
ihInterfaceTKCfgInfo
Pointer to Proficy Historian Collector Configuration Information. Use this if necessary to help determine the browse results. BrowsePosition
wchar_t
Pointer to a position of browsing for specific Tag. Recursive
ihTKBoolean
TRUE if the browse should be recursive in collector specific code. Applies only if your data source has a tree of available tags. DescriptionMask
wchar_t
* or a description mask that you should use when determining tags to return. SourceAddressMask
wchar_t
* or a source address mask that you should use when determining tags to return. CanReadASync
int
Non-zero if your collector is capable of asynchronous reads. Typically, this parameter does not affect browse results. DoMsgPump
int
0 should be ignored. NumSkipped
int
Use this to return any tags that were skipped because they did not match the description or source address mask or had an invalid data type.
ihCollectorToolkitInitializeCompleted
When this method is called by the collector shell, it indicates that the initialization is complete.
- Prototype
-
ihCollectorToolkitInitializeCompleted(void)
- Returns
- FALSE on success; collector should return FALSE.
ihCollectorToolkitInitialize
Use this interface to initialize the collector by using information in the
ihInterfaceTKCfgInfo
and
ihInterfaceTKPreCfgInfo
structures. Your code also needs to
save away the callback pointers passed into this function for use later with
unsolicited reads and browses.
- Prototype
-
int ihCollectorToolkitInitialize(ihInterfaceTKCfgInfo *Cfg, ihInterfaceTKPreCfgInfo *PreCfg, wchar_t *ErrorMsg, int ErrorMsgSize,wchar_t *RegKeyName, ihCollectorToolkitCollectorCallbacks *Callbacks, int DoDebug)
- Returns
-
TRUE if initialization was successful. Otherwise, FALSE. If initialization failed, you can return a text string error message in the
ErrorMsg
parameter and that message will be entered into the collector log. - Parameters
-
Name Data Type Description Cfg
ihInterfaceTKCfgInfo
Pointer to the Proficy Historian Collector Configuration Information. PreCfg
ihInterfaceTKPreCfgInfo
Pointer to the Collector pre-Configuration Information. ErrorMsg
wchar_t
Pointer to an Initialization Error Message, if any. Any error would be reported to collector log. ErrorMsgSize
int
Error Message Size. This is the maximum length that your error message size can be. RegKeyName
wchar_t
Pointer to a Registry Key Name. Will be filled in with the location of your collector???s registry information. Callbacks
ihTKCollectorCallbacks
Pointer to callbacks to functions inside the collector shell. Save these function pointers and call them at the appropriate time, such as to deliver unsolicited data into the shell. DoDebug
int
This value will be zero if the collector is not in debug mode and non-zero if debug mode is enabled. Save this value and use it to log more or less information to your collector log.
ihCollectorToolkitMiscReload
Reserved for future use. Your collector specific code should simply call the function
in the CCollectorDelegator
.
- Prototype
-
int ihCollectorToolkitMiscReload(ihTKTimeStruct *StartTime, ihTKTimeStruct *EndTime)
- Returns
-
TRUE; your collector specific code should return TRUE.
- Parameters
-
Name Data Type Description *StartTime
ihInterfaceTKTimeStruct
Reserved *EndTime
ihTKTimeStruct
Reserved
ihCollectorToolkitPolledAddTag
The collector shell calls this to indicate the tag will be used later in polled
collection. The collector specific code should keep all information given as it will
be used in the ihInterfaceGetData
call.
The polled tag add notification is done via
ihCollectorToolkitPolledAddTag
and data is sent to Historian
via ihCollectorToolkitGetData
. The frequency of asking for data for
polled tag is based on the tag collection interval.
- Prototype
-
int ihCollectorToolkitPolledAddTag(ihInterfaceTKPolledTagInfo *PolledTag, int IsCollectorStarting)
- Returns
- TRUE on success; your collector specific code should return TRUE.
- Parameters
-
Name Data Type Description PolledTag
ihInterfaceTKPolledTagInfo
Pointer to a Historian Collector Polled Tag Information. IsCollectorStarting
int
Parameter to provide information about collector state.
ihCollectorToolkitPreInitialize
Use this interface to provide the toolkit with some of the capabilities of the collector. Here, you can specify if you support multiple instances, if you support unsolicited reads, and if your collector supports browsing.
Information filled into the ihInterfaceTKCfgInfo
structure will
later be passed into the ihCollectorToolkitInitialize
function.
- Prototype
-
void ihCollectorToolkitPreInitialize(ihInterfaceTKPreCfgInfo *PreCfg, ihInterfaceTKCfgInfo *Cfg)
- Returns
- Void.
- Parameters
-
Name Data Type Description PreCfg
ihInterfaceTKPreCfgInfo
Pointer to Collector Configuration Information. Cfg
ihInterfaceTKCfgInfo
Pointer to additional Collector Configuration Information.
ihCollectorToolkitPropertyUpdate
This function is called when the user changes any collector property in Historian Administrator such as the General1 -5 properties. Your collector specific code can decide what changes are meaningful.
- Prototype
-
void ihCollectorToolkitPropertyUpdate(ihInterfaceTKCfgInfo *Cfg)
- Returns
- Void.
- Parameters
-
Name Data Type Description Cfg
ihInterfaceTKCfgInfo
Current values of Collector configuration information.
ihCollectorToolkitPolledInit
The collector shell calls this method at start up and on change to indicate the start
of a list of tags to be polled, as the collector runs. The actual polling takes
place in the ihInterfaceGetData
call.
- Prototype
-
int ihCollectorToolkitPolledInit(void);
- Returns
- FALSE on success; your collector specific code should return FALSE.
ihCollectorToolkitPolledInitCompleted
The collector shell will call this to indicate the end of the polled tag list. This informs the source to begin its initialization.
- Prototype
-
int ihCollectorToolkitPolledInitCompleted(void);
- Returns
- FALSE on success; your collector specific code should return FALSE.
ihCollectorToolkitPropertyUpdate
This function is called when the user changes any collector property in Historian Administrator such as the General1 -5 properties. Your collector specific code can decide what changes are meaningful.
- Prototype
-
void ihCollectorToolkitPropertyUpdate(ihInterfaceTKCfgInfo *Cfg)
- Returns
- Void.
- Parameters
-
Name Data Type Description Cfg
ihInterfaceTKCfgInfo
Current values of Collector configuration information.
ihCollectorToolkitPolledDeleteTag
The shell calls this function to notify the collector specific code that a tag will no longer be polled.
- Prototype
-
int ihCollectorToolkitPolledDeleteTag(int tagId);
- Returns
- TRUE on success; your collector specific code should return TRUE.
- Parameters
-
Name Data Type Description TagId
int
TagId that is being deleted. The tag name is not passed into this function. Match the TagId with the information passed in the ihCollectorToolkitPolledAddTag
.
ihCollectorToolkitPolledInitCompleted
The collector shell will call this to indicate the end of the polled tag list. This informs the source to begin its initialization.
- Prototype
-
int ihCollectorToolkitPolledInitCompleted(void);
- Returns
- FALSE on success; your collector specific code should return FALSE.
ihCollectorToolkitReset
The toolkit will call this function when the collector is being paused or shutdown. Proficy Historian stores collector information before the Collector is shut down.
- Prototype
-
void ihCollectorToolkitReset(int Shutdown)
- Returns
- Void.
- Parameters
-
Name Data Type Description Shutdown
int
0 if the collector pauses and non-zero if the collector is shutting down.
ihCollectorToolkitStartReading
When the shell calls this method, it indicates the collector specific code to start polled and unsolicited reading from the source.
- Prototype
-
int ihCollectorToolkitStartReading(void)
- Returns
- TRUE on success; your collector specific code should return TRUE.
ihCollectorToolkitShutdown
The collector shell will call this function when the collector executable
(.exe
) is shutting down.
- Prototype
-
void ihInterfaceTKShutdown(void);
- Returns
- Void.
ihCollectorToolkitTagChange
The toolkit will call this function when the properties of a tag are changed in Client Tools, Historian Administrator, or other external tools. The tag and what properties have changed are indicated in the tag props and changed fields.
This function is called on tag property change and is not involved with data changes.
Your collector should decide how to react to tag property changes or should ignore the changes.
- Prototype
-
int ihCollectorToolkitTagChange(int TagId, iHTKTagProperties *TagProps, iHTKTagFields *ChangedFields
- Returns
- int (TRUE/FALSE).
- Parameters
-
Name Data Type Description TagId
int
TagID that has changed. TagProps
ihTKTagProperties
Pointer to a Proficy Historian Tag Property structure that indicates the new tag property values. ChangedFields
ihTKTagFields
Pointer to information about which tag properties have changed.
ihCollectorToolkitGetEnumeratedSets
The toolkit calls this function based on the value configured under the
SynchInterval
registry key value. This function is called every
x minutes, where x is the value configured
for the registry key.
Collectors implemented using the Collector Toolkit have to implement this method to fetch the EnumeratedSet
from
their source.
- Prototype
-
int ihCollectorToolkitGetEnumeratedSets(ihTKEnumeratedSetRecordSet *EnumeratedSetRecordSet)
- Returns
- int (TRUE/FALSE).
- Parameters
-
Name Data Type Description EnumeratedSetRecordSet
ihTKEnumeratedSetRecordSet
Pointer to an EnumeratedSetRecordSet
structure which should be added to Historian Server.
ihCollectorToolkitWriteValue
The toolkit will call this function once per minute if the user has configured heartbeat/status/rate tags. If your collector does not support this feature you can hard code a return value and not do the write.
- Prototype
-
void ihCollectorToolkitWriteValue(wchar_t *Tag, wchar_t *SValue, double DValue
- Returns
- Void.
- Parameters
-
Name Data Type Description Tag
wchar_ t
Pointer to a source address in the data source to write to. doubled Value
DValue
Numeric value to be written, if the Tag is a numeric tag. For example, a report rate would be written to a rate tag or a 1 would be written to a heartbeat tag. SValue
SValue
The string value to be written if tag source address is a string tag. For example, the string Running would be written to a status tag.
What is a Helper Method?
Helper Methods are used to allocate memory for variables while developing Collectors. Using these helper methods will prevent cross boundary issues. The following are the Helper Methods:
Name | Description |
---|---|
wchar_t*TKStrdup(const wchar_t* string) |
Use this method to allocate memory on the heap, assign values and returns. |
voidTKFree(void* pointer) |
Use this method to free up pointer memory. |
void*TKMalloc(_In_ size_t _Size) |
Use this method to allocate memory. |