Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / Equals Method
An object to test.


In This Topic
    Equals Method (DataQuality)
    In This Topic
    Determines whether this instance is equal to the given object.
    Syntax
    Public Overrides Function Equals( _
       ByVal obj As System.Object _
    ) As System.Boolean
    public override System.bool Equals( 
       System.object obj
    )
    public:
    System.bool Equals( 
       System.Object^ obj
    ) override 

    Parameters

    obj
    An object to test.

    Return Value

    True if the specified object equals this instance.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also