Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / IsUserStatusValid Property


In This Topic
    IsUserStatusValid Property
    In This Topic
    Whether this instance contains user-status information.
    Syntax
    Public Property IsUserStatusValid As System.Boolean
    public System.bool IsUserStatusValid {get; set;}
    public:
    property System.bool IsUserStatusValid {
       System.bool get();
       void set (    System.bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also