Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / ReplacedMask Field


In This Topic
    ReplacedMask Field
    In This Topic
    Bit-mask for extracting replaced flag.
    Syntax
    Public Const ReplacedMask As System.UInteger
    public const System.uint ReplacedMask
    public:
    const System.uint ReplacedMask
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also