Name | Description | |
---|---|---|
![]() | DataCriteria Constructor | Overloaded. |
The following tables list the members exposed by DataCriteria.
Name | Description | |
---|---|---|
![]() | DataCriteria Constructor | Overloaded. |
Name | Description | |
---|---|---|
![]() | BackwardTimeOrder | Establish whether to resolve a query in backward time order (true) or forward time order (false). |
![]() | CalculationMode | Establish a calculation mode for a query. See DataCriteria.CalculationModeType. |
![]() | End | Establish an end time for a query. |
![]() | FilterComparisonMode | Establish a filter comparison mode for a query. See DataCriteria.FilterComparisonModeType. |
![]() | FilterComparisonValue | Establish a constant value to filter a query. This value is compared using FilterComparisonMode. |
![]() | FilterExpression | Provide a complete filter Expression to query on. This is independent of the FilterTag. When the Filterexpression is set a FilterComparisonMode or FilterComparisonValue should not be provided. e.g. (Testag1 > 5000) |
![]() | FilterMode | Establish a filter mode for a query. See DataCriteria.FilterModeType. |
![]() | FilterTag | Establish a tag name to filter a query. Filtered tag queries evaluate the value of the filter tag against a constant comparison value and only retain time intervals where this comparison evaluates true. Filtered tag queries are further modified by DataCriteria.FilterModeType and DataCriteria.FilterComparisonModeType. |
![]() | Interval | |
![]() | IntervalMicroseconds | Establish a number of milliseconds between data samples for a query. |
![]() | IntervalType | |
![]() | NumberOfSamples | Establish a number of data samples to retrieve for a query. |
![]() | QueryModifiers | Establish the QueryModifiers to a query. |
![]() | SamplingMode | Establish a sampling mode for a query. See DataCriteria.SamplingModeType. |
![]() | Start | Establish a start time for a query. |
![]() | StateValue | Establish a value to for the calculation mode Statevalue or StateCount. |
![]() | Tagnames | Establish a set of tag names for a query. |