Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataCriteria Class / NumberOfSamples Field


In This Topic
    NumberOfSamples Field
    In This Topic
    Establish a number of data samples to retrieve for a query.
    Syntax
    Public NumberOfSamples As System.UInteger
    public System.uint NumberOfSamples
    public:
    System.uint NumberOfSamples
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also